TOKEN DONE INTERRUPT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TOKEN DONE INTERRUPT

1,063 Views
Anirudh_007
Contributor I

Hi,

I am using k32l2a31vlh1a controller. in that i configured USB as VCOM and configured the clock as 48Mhz.

When i run the code, USB reset interrupt is happening and i configure the control endpoint but token done interrupt is not hitting and PC is not able to detect my board as well and this pop up appears with message(USB DEVICE IS NOT RECOGNIZED).

I use the same logic in k32l2a41vll1a evaluation board with same logic. in that board it is working but not in my custom board(k32l2a31vlh1a)

Any Help,

Thanks

Anirudh

0 Kudos
Reply
0 Replies