TOKEN DONE INTERRUPT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TOKEN DONE INTERRUPT

1,073件の閲覧回数
Anirudh_007
Contributor I

Hi,

I am using k32l2a31vlh1a controller. in that i configured USB as VCOM and configured the clock as 48Mhz.

When i run the code, USB reset interrupt is happening and i configure the control endpoint but token done interrupt is not hitting and PC is not able to detect my board as well and this pop up appears with message(USB DEVICE IS NOT RECOGNIZED).

I use the same logic in k32l2a41vll1a evaluation board with same logic. in that board it is working but not in my custom board(k32l2a31vlh1a)

Any Help,

Thanks

Anirudh

0 件の賞賛
返信
0 返答(返信)