SDK warnning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK warnning

1,644 Views
sw1234
Contributor I

Hello, I am creating a project with the K32L2B21 series.
I added the SDK library, but the warning appears as below

The SDK I have is only version 2.3, but MCUXpresso wants 2.2.
What should I do?
or 
Since my SDK is the top version, can I ignore that warnning?

 

 

Issue: Unsupported version of the ADC16 Driver in the toolchain/IDE project. Required: 2.2.0, actual: 2.3.0. Project might not compile correctly.
Level: Warning
Type: Validation
Tool: Toolchain/IDE project
Origin: Peripherals
Target: Toolchain/IDE project: core0
Resource: platform.drivers.adc16

(My MCUXpresso version is "MCUXpresso IDE v11.6.1_8255")

 

Thank you

Tags (1)
0 Kudos
Reply
1 Reply

1,503 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Generally, you can ignore the warning information.

But I suggest you download the latest MCUXPresso tools with version11.9

https://nxp.flexnetoperations.com/control/frse/product?entitlementId=204440247&lineNum=1&authContact...

and also download the latest SDK package.

https://mcuxpresso.nxp.com/en/welcome

and check if there is warning inf

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply