Parallel execution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,582件の閲覧回数
Trento
Contributor I

Hi all,

is it possible to execute functions on different cores (K32LA6 CM0 and CM4) in parallel, I mean asynchronously? If so, how to implement that?

Thanks in advance!

Best regards

0 件の賞賛
返信
1 解決策
3,554件の閲覧回数
chris_brown
NXP Employee
NXP Employee

Hi Trento,

Yes, this is possible.  You are talking about dual core operation.  Have a look at the multicore examples from the SDK for the K32L3A6.  There is also this application note:  Dual-core project creation and conversion for K32L3A6 devices 

Best regards,

Chris 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,555件の閲覧回数
chris_brown
NXP Employee
NXP Employee

Hi Trento,

Yes, this is possible.  You are talking about dual core operation.  Have a look at the multicore examples from the SDK for the K32L3A6.  There is also this application note:  Dual-core project creation and conversion for K32L3A6 devices 

Best regards,

Chris 

0 件の賞賛
返信
3,549件の閲覧回数
Trento
Contributor I

Hi Chris,

thanks!

0 件の賞賛
返信