KinetisFlashTool download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KinetisFlashTool download

2,004 Views
sw1234
Contributor I

Hello.
I want to download the KinetisFlashTool.
But I don't know where to download it.
Can you tell me where it is?

sw1234_0-1704636993708.png


Thank you.

0 Kudos
Reply
1 Reply

1,852 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, pls refer to section Chapter 26 Kinetis ROM Bootloader in K32L3ARM.pdf, which can be  downloaded from the link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

In other words, there is ROM bootloader, it is not necessary to load flashloader to the flash, you can use blhost to connect to the K32 directly.

You can use above tools to download application code in the ROM boot process.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply