K32W041 - fsl_flash.* Flash_Program() - How to use multiple times in 1 FLASH_PAGE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W041 - fsl_flash.* Flash_Program() - How to use multiple times in 1 FLASH_PAGE

1,436 Views
Emiel1984
Contributor II

The issue:
I can't seem to figure out how to write\read Flash when there is less then a FLASH page (512 bytes) to be written. I want to write multiple records in a single page without the need to write them all at once.
So far I have not been able to succeed.




My Code:

 

 

 

 

 

uint8_t *data= "pointer to datastructure of 100 bytes";

for(i=0;i<100;i++)
{
  data[i] = i;//Put 0 upto 99..
}

//Request flash storing
StoreData(&data[0]);
StoreData(&data[0]);
StoreData(&data[0]);
StoreData(&data[0]);
#include "fsl_flash.h"
#define START_FLASH_STORAGE        (0x00059000)
uint32_t au32DataCopy[STORE_DATA_SIZE];
uint32_t au32DataCopy2[STORE_DATA_SIZE];

unsigned long FlashBufferHead=0;

PUBLIC bool StoreData(uint8_t *inp)
{
    uint32_t *pu32Start = (uint32_t *)(START_FLASH_STORAGE+FlashBufferHead);

    uint8_t *data=(uint8_t*)&inp[0];
    uint8_t *datacopy=(uint8_t*)&au32DataCopy[0];
    uint8_t *datacopy2=(uint8_t*)&au32DataCopy2[0];
    flash_status_t driver_result;
    uint32_t i, u32StartPage;

    Initialize_FlashCircBuffer();

    /* erase sector if first write in new page */
    if (FlashBufferHead % 512 == 0)
    {
        u32StartPage = (uint32)pu32Start;
        u32StartPage /= 512;

        LOG_ERROR("Erase page: % d", u32StartPage);
        driver_result = FLASH_ErasePages(FLASH, u32StartPage, 1);

        if (driver_result != kStatus_FLASH_Success)
        {
            LOG_ERROR("Flash read unsuccessful");
        }
    }

    driver_result = FLASH_Program(FLASH, pu32Start, (uint32_t*)inp, 100);
    if (driver_result != kStatus_FLASH_Success)
    {
        LOG_ERROR("Flash read unsuccessful");
    }

    /* Read back data */
    uint32_t temp[4];
    for (i = 0; i < 100; i += 4)
    {
        FLASH_Read(FLASH, (uint8_t *)(pu32Start + i), 0, (uint32_t *)temp);
        memcpy(&au32DataCopy[i], (void *)temp, sizeof(temp));
    }

    /* Read back data again---debug issue  */
    for (i = 0; i < 100; i += 4)
    {
        FLASH_Read(FLASH, (uint8_t *)(START_FLASH_STORAGE + i), 0, (uint32_t *)temp);
        memcpy(&au32DataCopy2[i], (void *)temp, sizeof(temp));
    }

    /* determine if saved correctly */
    for (i = 0; i < 100; i++)
    {
        if(data[i] != datacopy[i])
        {
            LOG_ERROR("Flash verify unsuccessful");
        }

    }

    LOG_ERROR("verify completed..?");

    FlashBufferHead +=100;
}

 

 

 

 

 



Result:

At first I was increasing my flash location pointer by 100 (using FlashBufferHead ) during each run to allow a multiple of 100 bytes per pages to be saved. The second run I notice an offset in the values read. The values written are there, but seem to start 4 bytes later. I expected to be able to write at least in multiples of 4 bytes.

(...sorry my mcuxpresso is really buggy now... no screenshot yet...)


If I'm increasing pointer to flash by 256. The second run byte 35 is always read back as a different value then was requested to write. All other 100 bytes are written\read correctly.

Emiel1984_0-1659644286866.png


If I'm increasing my flash location pointer by 512, this always results in a FLASH_ErasePages call before each write. Then there are no issues.

Code from fsl_flash.c

 

 

 

 

 

int FLASH_Program(FLASH_Type *pFLASH, uint32_t *pu32Start, uint32_t *pu32Data, uint32_t u32Length)
{
    int status = 0;

    uint32_t end  = (uint32_t)pu32Start + u32Length;

    uint32_t padding  = (FLASH_PAGE_SIZE - (end & (FLASH_PAGE_SIZE-1))) & (FLASH_PAGE_SIZE-1);

    pFLASH->INT_CLR_STATUS = FLASH_STAT_ALL;

    pFLASH->AUTOPROG = FLASH_AUTO_PAGE;

    memcpy(pu32Start, pu32Data, u32Length);

    while (padding-- > 0)
    {
        *(uint8_t*)end ++ = 0;
    }

    status = FLASH_Wait(pFLASH);

    pFLASH->AUTOPROG = FLASH_AUTO_OFF;

    return status;
}

 

 

 

 

 

 

0 Kudos
Reply
0 Replies