K32L2B3 SWD Pin Overwrite - Debug error: 02: failed on connect could not connect to core

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K32L2B3 SWD Pin Overwrite - Debug error: 02: failed on connect could not connect to core

2,020 次查看
JonCan
Contributor I

Hi everyone,

 

I just started working with a Freedom Development Board for the K32L2B3 MCU series (https://www.nxp.com/design/development-boards/freedom-development-boards/mcu-boards/nxp-freedom-deve...).

During some tests, the SWD(PTA3 Pin) got multiplexed as GPIO. After this, the debugger does not seem to connect properly anymore (i.e. I cannot reprogram the device). The error that I receive is: "02: failed on connect could not connect to core" as soon as I click on debug with one of the SDK example programs (these worked fine in the beginning).

I tried holding the reset button during the debug sequence, but this gives the error: "Cannot halt processor Failed on chip setup: Ep(04). Cannot halt processor."

 

Is there any way to reset the SWD Pin functionality on the K32L2B3 series?

 

Many thanks.

0 项奖励
回复
0 回复数