FB Clock Output not rectangular

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FB Clock Output not rectangular

ソリューションへジャンプ
4,743件の閲覧回数
Kolibri
Contributor III

Hello i´m working with the Development Board FRDMK32L3A6 and i want to use the FB_CLKOUT Pin to clock another Board. Here in this pictures are the settings i use.

Clock_Diagram_FRDMK32L3A6.pngClock_Diagram_FRDMK32L3A6.png

Clock_Pin_FRDMK32L3A6.pngClock_Pin_FRDMK32L3A6.png

Now i´ve measured the Clock Signal with an Oscilloscope and this is what i get. Am i doing something wrong on my measurement or does the clock signal look like this? How can i change it to be rectangular?

CLOCK.pngCLOCK.png

Thanks and best regards

タグ(1)
0 件の賞賛
返信
1 解決策
4,706件の閲覧回数
Kolibri
Contributor III

The clock signal never looks like a perfect squarewave and it works fine like it is.

Best regards Kolibri

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,734件の閲覧回数
Kolibri
Contributor III

I think i got it, i have to add a series resistor to the signal i will try it tomorrow.

0 件の賞賛
返信
4,729件の閲覧回数
Kolibri
Contributor III

I´ve tried now with different resistors, the signal changes but it´s not gettin rectangular. Can someone please help me to solve this problem. Is there a formula to calculate the series resistor or is it even needed?

Thanks and best regards

0 件の賞賛
返信
4,707件の閲覧回数
Kolibri
Contributor III

The clock signal never looks like a perfect squarewave and it works fine like it is.

Best regards Kolibri

0 件の賞賛
返信