QGC PX4 Firmware Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QGC PX4 Firmware Issue

ソリューションへジャンプ
6,372件の閲覧回数
loganlamm17
Contributor II

Hello,

I recently finished uploading the bootloader and JLink debugging code into the FMU. I followed the process that was provided by the NXP Hovergames drone tutorial, and downloaded the QGC software to connect to the drone; thus input individual code with MAVLink. However, I ran into an issue with trying to upgrade the firmware and connect to the software. The message came up where the FMU time-ed out trying to connect to the software. I believe one issue is that I haven't used an updated QGC application since I downloaded it in October of 2021. I used the same bin codes from the NXP site, so I don't believe there is an issue with the binary codes for the firmware. What is the possible solution to this? I am so close to completing my project, and I don't want to be held back because of this.

タグ(5)
0 件の賞賛
返信
1 解決策
6,338件の閲覧回数
loganlamm17
Contributor II

I was able to retry installing the bootloader via the JLink debugger. I made sure to write 0x0 after including the file name for the loadbin command. This fixed the issue of connecting the FMU to the QGC Software.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
6,353件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Does the Troubleshooting fix this issue? I will move this question to HoverGames Drone Challenge community.

Best Regards,
Robin

0 件の賞賛
返信
6,339件の閲覧回数
loganlamm17
Contributor II

I was able to retry installing the bootloader via the JLink debugger. I made sure to write 0x0 after including the file name for the loadbin command. This fixed the issue of connecting the FMU to the QGC Software.

 

0 件の賞賛
返信