FMU broken - cannot erase or program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FMU broken - cannot erase or program

6,754 Views
manuel_iglesias
Contributor II

Hello,

I am trying to erase the FMU board that came on the HoverGames3 kit and I am getting issues of protected device and J-Link or J-Flash both fails.

The original post is here

Trying with J-Flash also fails as shown in the attachment .Segger can read the whole device no problem and comms seems ok. 

I am using J-Link PLUS with J-Flash as the little mini edu thing won't have the license to use with it.

What could be wrong?

 

0 Kudos
Reply
2 Replies

6,517 Views
iaingalloway
NXP Employee
NXP Employee

Summary - Normally for the FMU there is a bootloader file written to 0x0000 and then a program file at 0x6000.  It is believed that the program file was accidentally written to 0x6000 AND that this particular compilation did coincidentally have the security bits flashed.
The unlocking may not have worked in this instance:
https://forum.segger.com/index.php/Thread/2390-JLink-on-unsecure-and-erase-Kinetis-FLASH/

 

0 Kudos
Reply

6,727 Views
NXPAmar
NXP Employee
NXP Employee

Hello, 

have you tried flashing the firmware using the QGroundControl Software (Firmware - NXP HoverGames (gitbook.io)) ? 

I also built the Bootloader myself following this part of our documentation: Building the bootloader - NXP HoverGames (gitbook.io)

 

Might I also invite you to come join the Hackster Discord Server, where many of the discussions around HoverGames are taking place: https://discord.gg/3bcCEYTFz7 

 

Kind Regards 

Amar

0 Kudos
Reply