FMU broken - cannot erase or program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FMU broken - cannot erase or program

6,802件の閲覧回数
manuel_iglesias
Contributor II

Hello,

I am trying to erase the FMU board that came on the HoverGames3 kit and I am getting issues of protected device and J-Link or J-Flash both fails.

The original post is here

Trying with J-Flash also fails as shown in the attachment .Segger can read the whole device no problem and comms seems ok. 

I am using J-Link PLUS with J-Flash as the little mini edu thing won't have the license to use with it.

What could be wrong?

 

0 件の賞賛
返信
2 返答(返信)

6,565件の閲覧回数
iaingalloway
NXP Employee
NXP Employee

Summary - Normally for the FMU there is a bootloader file written to 0x0000 and then a program file at 0x6000.  It is believed that the program file was accidentally written to 0x6000 AND that this particular compilation did coincidentally have the security bits flashed.
The unlocking may not have worked in this instance:
https://forum.segger.com/index.php/Thread/2390-JLink-on-unsecure-and-erase-Kinetis-FLASH/

 

0 件の賞賛
返信

6,775件の閲覧回数
NXPAmar
NXP Employee
NXP Employee

Hello, 

have you tried flashing the firmware using the QGroundControl Software (Firmware - NXP HoverGames (gitbook.io)) ? 

I also built the Bootloader myself following this part of our documentation: Building the bootloader - NXP HoverGames (gitbook.io)

 

Might I also invite you to come join the Hackster Discord Server, where many of the discussions around HoverGames are taking place: https://discord.gg/3bcCEYTFz7 

 

Kind Regards 

Amar

0 件の賞賛
返信