Unused NVT4858 CLK_FB Pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unused NVT4858 CLK_FB Pin

ソリューションへジャンプ
2,300件の閲覧回数
JsGraaf
Contributor II

Hello, 

I was wondering what the spec is when the CLK_FB pin is not used. My MCU (STM32U5A9) doesn't have a feedback pin for the SDMMC interface. Do I have to connect it to prevent noise? 

 

Kind Regards,

 

Joris

0 件の賞賛
返信
1 解決策
2,288件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Joris,

The NVT4858's CLK_FB pin is used for clock synchronization, but if your MCU does not have a feedback pin for the SDMMC interface, you can leave the CLK_FB pin unconnected. The NVT4858 is designed to handle such scenarios without causing issues.

However, to minimize potential noise, ensure that your layout follows good design practices, such as keeping traces short and well-routed and using proper grounding techniques.

BRs, Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,289件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Joris,

The NVT4858's CLK_FB pin is used for clock synchronization, but if your MCU does not have a feedback pin for the SDMMC interface, you can leave the CLK_FB pin unconnected. The NVT4858 is designed to handle such scenarios without causing issues.

However, to minimize potential noise, ensure that your layout follows good design practices, such as keeping traces short and well-routed and using proper grounding techniques.

BRs, Tomas

0 件の賞賛
返信
2,285件の閲覧回数
JsGraaf
Contributor II

Thank you for your swift response! I have a solid ground plane directly under the signal layers (each lines passes to the other side once), all the traces are spaced more the 0.4mm apart and the trace lenghts are within 7mm of each other (max len is 44mm). The only part of the spec I have not adhered to is the 50 ohm impedance lines (mine are around 63 ohm). I will be running the interface at 48 Mhz 4-bit mode. Will this be possible without the controlled impedance?

Kind Regards,

 

Joris

タグ(1)
0 件の賞賛
返信
2,261件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Joris,

Running the interface at 48MHz in 4-bit mode with 63Ω impedance lines should be feasible. I would not expect signal integrity issues, considering your short traces and good layout.

If you ever plan to run higher-speed SDMMC modes in the future, then controlled 50Ω impedance, better trace matching and using CLK_FB might become more critical. But for 48 MHz 4-bit, your setup should work without problems.

BRs, Tomas

0 件の賞賛
返信
2,245件の閲覧回数
JsGraaf
Contributor II

Hello Tomas,

Again thank you for all your help!

Kind Regards,

Joris

タグ(1)
0 件の賞賛
返信