MC33772B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33772B

937件の閲覧回数
kevinyue
Contributor I

Here's the thing: We were going to use the MC33772B device for development, but we bought the MC33772C device again because of the lack of information, but our hardware is ready. I want to verify the state of our circuit communication; if I use the instruction MC33772C to read the 0 address register to send to the MC33772B device, can I get a valid callback? At the moment I can only receive all 0s.

 

0 件の賞賛
返信
1 返信

912件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Rick,

The MC33772C introduces several changes in the communication protocol and physical layer that make it incompatible with the MC33772B at the communication level. So if your SW is designed for MC33772B and you are using MC33772C devices, the communication will not function correctly unless the software and possibly some external components are updated to support the MC33772C protocol and architecture. Please refer to the AN12633 for more details. 

BRs, Tomas

0 件の賞賛
返信