VL82C420 Datasheet missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VL82C420 Datasheet missing

2,753件の閲覧回数
Mike1978uk
Contributor I

I’m seeking information pertaining to the above VLSI chipset

i’ve searched the web to find details of the pin connections and this was used in  number of notebooks using the 486SL CPU

It was part of the SCAMP IV Chipset

VLSI Technology’s notebook chips include the 82C420 System Controller, 82C144 Peripheral Controller, 82C146 PCMCIA

Controller, and the 82C170 LCD Graphics Accelerator. VLSI’s ML Bus is time-multiplexed onto the low 16 bits of the local bus.

I am knocking every door to find the datasheet for the VL82C420

It is known the chip was used in the following notebooks in the 90’s

AST Ascentia 910N
Compaq Lte Elite 4/50CX, 4/75C, 75CX, 75CX
IBM Thinkpad 230Cs
IBM Palmtop PC110

If anyone has the datasheet or pinout then please contact me.

Thanks Mike

 

ラベル(2)
タグ(4)
1 返信

2,415件の閲覧回数
zikolas
Contributor I

I've also been trying to find the data-sheet for the VL82C420. Appreciate it's before NXP's time but hopefully it's in a vault somewhere, it would be immensely helpful to have it.

Cheers, Nick.

0 件の賞賛
返信