[PCA9552] connecting multiple LED on 1 pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[PCA9552] connecting multiple LED on 1 pin

ソリューションへジャンプ
1,304件の閲覧回数
Kitta
Contributor I

Hi,

I want to use 24 pcs of LED and make this synchronixed blink.

 In Application note "AN264.pdf" p24, it seems that I can connect multiple LED in one pin if I use external FET or a bipolar transistor. (each pin under 25mA, 100mA in total) I don't quite understand this FET or bipolar transistor connection.

Could you explain how I can do this? By doing so, would it be possible to control each LED individually? 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,291件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Emiko,

each channel can be controlled individually. If you connect more LEDs to one channel, you will not be able to control each LED connected to this channel individually. 

JozefKozon_0-1720436116891.png

The LEDs above cannot be controlled individually. 

The LEDs below can be controlled individually.

JozefKozon_1-1720436182637.png

If you want to connect more LEDs to one channel, please use a bipolar transistor. 

JozefKozon_2-1720436281961.png

However we also have 24 channels LED controllers. E.g. PCA9956B with I2C interface or PCA9957HN with SPI interface. Please refer to this link for our LED controllers portfolio. 

JozefKozon_3-1720436470018.png

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,292件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Emiko,

each channel can be controlled individually. If you connect more LEDs to one channel, you will not be able to control each LED connected to this channel individually. 

JozefKozon_0-1720436116891.png

The LEDs above cannot be controlled individually. 

The LEDs below can be controlled individually.

JozefKozon_1-1720436182637.png

If you want to connect more LEDs to one channel, please use a bipolar transistor. 

JozefKozon_2-1720436281961.png

However we also have 24 channels LED controllers. E.g. PCA9956B with I2C interface or PCA9957HN with SPI interface. Please refer to this link for our LED controllers portfolio. 

JozefKozon_3-1720436470018.png

With Best Regards,

Jozef

0 件の賞賛
返信