[PCA9552] connecting multiple LED on 1 pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[PCA9552] connecting multiple LED on 1 pin

Jump to solution
1,289 Views
Kitta
Contributor I

Hi,

I want to use 24 pcs of LED and make this synchronixed blink.

 In Application note "AN264.pdf" p24, it seems that I can connect multiple LED in one pin if I use external FET or a bipolar transistor. (each pin under 25mA, 100mA in total) I don't quite understand this FET or bipolar transistor connection.

Could you explain how I can do this? By doing so, would it be possible to control each LED individually? 

Labels (1)
0 Kudos
Reply
1 Solution
1,276 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Emiko,

each channel can be controlled individually. If you connect more LEDs to one channel, you will not be able to control each LED connected to this channel individually. 

JozefKozon_0-1720436116891.png

The LEDs above cannot be controlled individually. 

The LEDs below can be controlled individually.

JozefKozon_1-1720436182637.png

If you want to connect more LEDs to one channel, please use a bipolar transistor. 

JozefKozon_2-1720436281961.png

However we also have 24 channels LED controllers. E.g. PCA9956B with I2C interface or PCA9957HN with SPI interface. Please refer to this link for our LED controllers portfolio. 

JozefKozon_3-1720436470018.png

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
1 Reply
1,277 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Emiko,

each channel can be controlled individually. If you connect more LEDs to one channel, you will not be able to control each LED connected to this channel individually. 

JozefKozon_0-1720436116891.png

The LEDs above cannot be controlled individually. 

The LEDs below can be controlled individually.

JozefKozon_1-1720436182637.png

If you want to connect more LEDs to one channel, please use a bipolar transistor. 

JozefKozon_2-1720436281961.png

However we also have 24 channels LED controllers. E.g. PCA9956B with I2C interface or PCA9957HN with SPI interface. Please refer to this link for our LED controllers portfolio. 

JozefKozon_3-1720436470018.png

With Best Regards,

Jozef

0 Kudos
Reply