Is an external clock generator required when using SerDes in the S32Gx Familly?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is an external clock generator required when using SerDes in the S32Gx Familly?

899件の閲覧回数
Ralph88
Contributor II

Hi, all

When designing circuits with the S32Gx Family, is an external clock generator required for using SerDes?

I am curious if it is possible to use only the internal PLL without an external clock generator.

 

Thanks and best regards

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

887件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Ralph88 

Thanks for your post.

An external reference clock is required which meets PCIe Gen3 clock specifications.

If PCIe Gen3 is not required in your design, The internal reference clock can be used for supporting PCIe Gen2 and SGMII communication.

I hope it will help.

 

BR

Chenyin

 

0 件の賞賛
返信