Is an external clock generator required when using SerDes in the S32Gx Familly?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is an external clock generator required when using SerDes in the S32Gx Familly?

1,945 Views
Ralph88
Contributor II

Hi, all

When designing circuits with the S32Gx Family, is an external clock generator required for using SerDes?

I am curious if it is possible to use only the internal PLL without an external clock generator.

 

Thanks and best regards

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,933 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Ralph88 

Thanks for your post.

An external reference clock is required which meets PCIe Gen3 clock specifications.

If PCIe Gen3 is not required in your design, The internal reference clock can be used for supporting PCIe Gen2 and SGMII communication.

I hope it will help.

 

BR

Chenyin

 

0 Kudos
Reply