Why would the 5V connection with the TB switch on a TWR-ELEV primary board not work?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why would the 5V connection with the TB switch on a TWR-ELEV primary board not work?

3,087件の閲覧回数
jessicacollins
Contributor I

I have been trying to connect 5V from an external source to the primary elevator board and when I move the switch from OFF to TB it doesn't turn on. The current goes high and the voltage goes low (it measures 160 ohms without power connected when I move the switch to the TB selection too). There is no issue when i connect via USB and have it on that switch.

I am trying to build a robotic car for school following poorly written instructions and have been unable to get the tower to work off ~5V supplied via batteries. As of right now I can only get ti to function with the USB cable connected to my computer. I need it to work through the J10 connector and the batteries.

0 件の賞賛
返信
0 返答(返信)