Implementing AI/ML on KW45B41Z-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing AI/ML on KW45B41Z-EVK

360 Views
Srushti_Mulimani
Contributor I

Hi NXP Community,

I am working on an edge AI application for the KW45B41Z-EVK (Cortex-M33) and would like advice on deploying a machine learning model on this board.

Since the KW45 SDK does not include the eIQ/TFLM middleware by default, my plan is:

  1. Model Training: Train an n-class classification model for time-series data using eIQ Time Series Studio (eIQ TSS). Since the KW45 is not listed as a target in eIQ TSS, I selected the FRDM-MCXN947 (Cortex-M33) as the target platform to export the model.

  2. Runtime Deployment: Port the middleware/eiq/tensorflow-lite folder from the FRDM-MCXN947 SDK into my KW45 SDK project and link it with CMSIS-NN.

My Questions:

  • Is porting the eIQ TFLM middleware from the MCXN947 SDK to the KW45 SDK a valid and supported approach?

  • Is selecting the FRDM-MCXN947 in eIQ TSS suitable for generating models to run on the KW45?

  • Is there any other recommended or native workflow to implement AI/ML on the KW45B41Z-EVK?

Thanks for your help!
KW45B41Z-EVK KW45 EIQ-TFLITE-MICRO EIQ-TOOLKIT #AIML 

0 Kudos
Reply
1 Reply

282 Views
sofiaurueta
NXP Employee
NXP Employee

Hello, hope you are doing well.

If you are using eIQ Time Series Studio (TSS), I would recommend porting your project from the FRDM-MCXW71 instead. It is an officially supported target in eIQ TSS and is software compatible with the KW45. Both devices share the same Cortex-M33 core architecture and a similar memory profile, so the generated library should be a much closer match for your hardware.

When using a device with such a different hardware profile as the FRDM-MCXN947 as a target for porting, there is a risk of generating incompatible models, for example, due to the differences in available RAM between both devices, or the generation of NPU-accelerated models specific to the MCXN947.

 

Hope this helps!

 

Best regards,
Sofia.

0 Kudos
Reply