ALSA error running eiq_genai_flow with ASR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ALSA error running eiq_genai_flow with ASR

94 次查看
herveld
Contributor I

Hello,

I am getting the following ALSA error when running eiq_genai_flow with asr enabled:

./eiq_genai_flow -i kasr --output-mode text
Target Device: i.MX95

ASR model used: whisper-small.en
LLM used: danube-onnx

##### Press Enter to start ASR #####
I'm listening!
ALSA lib /usr/src/debug/alsa-lib/1.2.12/src/confmisc.c:855:(parse_card) cannot find card 'default'
ALSA lib /usr/src/debug/alsa-lib/1.2.12/src/conf.c:5204:(_snd_config_evaluate) function snd_func_card_inum returned error: No such device
ALSA lib /usr/src/debug/alsa-lib/1.2.12/src/confmisc.c:422:(snd_func_concat) error evaluating strings
ALSA lib /usr/src/debug/alsa-lib/1.2.12/src/conf.c:5204:(_snd_config_evaluate) function snd_func_concat returned error: No such device
ALSA lib /usr/src/debug/alsa-lib/1.2.12/src/confmisc.c:1342:(snd_func_refer) error evaluating name
ALSA lib /usr/src/debug/alsa-lib/1.2.12/src/conf.c:5204:(_snd_config_evaluate) function snd_func_refer returned error: No such device
ALSA lib /usr/src/debug/alsa-lib/1.2.12/src/conf.c:5727:(snd_config_expand) Evaluate error: No such device
ALSA lib /usr/src/debug/alsa-lib/1.2.12/src/pcm/pcm.c:2722:(snd_pcm_open_noupdate) Unknown PCM sysdefault:CARD=default
Exception in thread audio_capture_thread:
Traceback (most recent call last):
File "threading.py", line 1075, in _bootstrap_inner
File "threading.py", line 1012, in run
File "asr/streaming/audio_capture.py", line 90, in capture_audio
File "asr/streaming/audio_capture.py", line 69, in open_pcm_device
alsaaudio.ALSAAudioError: No such device [sysdefault:CARD=default]

Both arecord and aplay are functional.

Here are the output of arecord:

arecord -l
**** List of CAPTURE Hardware Devices ****
card 0: wm8904audio [wm8904-audio], device 0: sai-tx-rx-wm8904-hifi wm8904-hifi-0 [sai-tx-rx-wm8904-hifi wm8904-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0

arecord -L
null
Discard all samples (playback) or generate zero samples (capture)
default:CARD=wm8904audio
wm8904-audio, sai-tx-rx-wm8904-hifi wm8904-hifi-0
Default Audio Device
sysdefault:CARD=wm8904audio
wm8904-audio, sai-tx-rx-wm8904-hifi wm8904-hifi-0
Default Audio Device


Is there a way to configure the default audio card for eiq_genai_flow ?

Best regards,
Hervé

0 项奖励
回复
0 回复数