mingw32-make run failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mingw32-make run failed

20,560件の閲覧回数
moticsoft
Contributor I

请教:

Gui_Guider 1.5.0 , 模拟器,选择C语音,然后出现提示: mingw32-make run failed ,应当如何解决?

0 件の賞賛
返信
20 返答(返信)

14,062件の閲覧回数
DING-YI
Contributor I

先点击编译部署c试试,我点完就可以了

0 件の賞賛
返信

20,115件の閲覧回数
Angle145
Contributor I

管理员身份运行打开软件就可以了

0 件の賞賛
返信

20,050件の閲覧回数
bigheadJano
Contributor I
我尝试过用管理员身份运行,还是一样会提示错误
0 件の賞賛
返信

20,038件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

Hi bigheadJano

    Can you check the java version on your host? if it is lower than 1.8.

please upgrade the Java version to 1.8.0 or higher, Reopen the GUIGuider and rebuild this project. if it still doesn't work, Please share the test project for debugging. Thank you very much for your support. BR Liubin

0 件の賞賛
返信

20,282件の閲覧回数
醒时笑
Contributor I

Is this problem solved? Now, also experiencing the same issue.

0 件の賞賛
返信

20,276件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

In order to better reproduce the problem, please provide the following information:

  1. host OS
  2. project created version(1.5.0 or other version)
  3. Is there a 'make' in the system environment variable? 
  4. would you share the error log info? 
  5. v7 work fine, but v8 failed, all right?

Best Regards

Liubin

0 件の賞賛
返信

20,274件の閲覧回数
醒时笑
Contributor I

操作系统使用 win10,创建 8.3 版本时出错,7.x 版本正常,系统环境变量有 make 编译器。

0 件の賞賛
返信

20,258件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

Can you build this project by command line mode?  Please follow blew steps:

  1. cd {project path}/lvgl-simulator
  2. make -r -j4;

And would you please share the full build log? Thanks 

Best Regards

Liubin

0 件の賞賛
返信

20,250件の閲覧回数
醒时笑
Contributor I

C:\Users\admin\Desktop\test\demo\lvgl-simulator>make
"Linking simulator.exe"
build/object/main.o:main.c:(.text.startup+0xf5): undefined reference to `video_play'
build/object/main.o:main.c:(.text.startup+0x109): undefined reference to `__mingw_sleep'
d:/program files (x86)/mingw/bin/../lib/gcc/mingw32/4.8.1/../../../../mingw32/bin/ld.exe: build/object/main.o: bad reloc address 0x20 in section `.eh_frame'
d:/program files (x86)/mingw/bin/../lib/gcc/mingw32/4.8.1/../../../../mingw32/bin/ld.exe: final link failed: Invalid operation
collect2.exe: error: ld returned 1 exit status
Makefile:112: recipe for target 'default' failed
make: *** [default] Error 1

0 件の賞賛
返信

20,244件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

Can you check the java version on your host? if it is lower than 1.8,

  1. please upgrade the Java version to 1.8.0 or higher,
  2. Reopen the GUIGuider and rebuild this project.

if it still doesn't work, Please share the test project for debugging. Thank you very much for your support.

BR 

Liubin

0 件の賞賛
返信

20,227件の閲覧回数
醒时笑
Contributor I

这是Python版本。Python 3.11.2 (tags/v3.11.2:878ead1, Feb 7 2023, 16:38:35) [MSC v.1934 64 位 (AMD64)] 在 win32 上”

下面是测试演示。

0 件の賞賛
返信

20,217件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

According to checking your test project, I found that the code of GUI GUIder is not generated, it should be the problem with the version of JAVA,  Would you check your java version? 


Best Regards

Liubin

0 件の賞賛
返信

20,210件の閲覧回数
醒时笑
Contributor I

更换成 Python 3.10.10 (tags/v3.10.10:aad5f6a, Feb 7 2023, 17:20:36) [MSC v.1929 64 bit (AMD64)] on win32还是有相同的问题.

0 件の賞賛
返信

20,199件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

是java 版本不能低于1.8, 不是python 版本。请您检查一下您系统中安装的java 版本

0 件の賞賛
返信

20,514件の閲覧回数
TieNiu
Contributor I

"Compiling C:/NXP/GUI-Guider-Projects/cc12/lvgl-simulator/../generated/gui_guider.c" "Compiling C:/NXP/GUI-Guider-Projects/cc12/lvgl-simulator/../generated/events_init.c" "Compiling C:/NXP/GUI-Guider-Projects/cc12/lvgl-simulator/../custom/custom.c" main.c: In function 'main': main.c:76:9: warning: implicit declaration of function 'video_play' [-Wimplicit-function-declaration] 76 | video_play(&guider_ui); | ^~~~~~~~~~ "Linking simulator.exe" ' collect2.exe: error: ld returned 1 exit status mingw32-make: *** [default] Error 1 Makefile:112: recipe for target 'default' failed

0 件の賞賛
返信

20,445件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @TieNiu 

 

Could you please take a screenshot show your steps, thanks!

 

BR

Alice

0 件の賞賛
返信

20,399件の閲覧回数
moticsoft
Contributor I

error.pngerror.png

0 件の賞賛
返信

20,242件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

I guess your problem is caused by the wrong generated code, please check your java version. It cannot be lower than 1.8. would you check the generated code status? 

Best regards

Liubin

0 件の賞賛
返信

20,530件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @moticsoft 

Could you please show your step, I will reproduce it on my side.

 

BR

Alice

0 件の賞賛
返信

20,512件の閲覧回数
TieNiu
Contributor I
我也遇到同样的问题 v7是正常的 v8会报下面错误



"Compiling C:/NXP/GUI-Guider-Projects/cc12/lvgl-simulator/../generated/gui_guider.c"
"Compiling C:/NXP/GUI-Guider-Projects/cc12/lvgl-simulator/../generated/events_init.c"
"Compiling C:/NXP/GUI-Guider-Projects/cc12/lvgl-simulator/../custom/custom.c"
main.c: In function 'main':
main.c:76:9: warning: implicit declaration of function 'video_play' [-Wimplicit-function-declaration]
76 | video_play(&guider_ui);
| ^~~~~~~~~~
"Linking simulator.exe"
'
collect2.exe: error: ld returned 1 exit status
mingw32-make: *** [default] Error 1
Makefile:112: recipe for target 'default' failed


0 件の賞賛
返信