how can I use lvgl7 when using version 1.8?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can I use lvgl7 when using version 1.8?

1,477 Views
ameng
Contributor I

When I use the lvgl8 version, the screen refresh rate is relatively low.

When I switch back to lvgl7, the refresh rate goes up,

so I still want to use lvgl7, but the guider 1.8 version does not have the lvgl project template.

Tags (1)
0 Kudos
Reply
2 Replies

1,447 Views
WenbinYuan
NXP Employee
NXP Employee

Hi @ameng,

 

Since the LVGL V7.10.1 in GUI Guider has seen minimal updates in recent releases, you can effectively utilize GUI Guider V1.7.2 to construct V7 projects that include all available features.

 

Best Regards,

Wenbin 

0 Kudos
Reply

1,425 Views
ameng
Contributor I
Thank you. Because version 1.8 has the function of control locking, I want to use this function. Thank you. This software is very good.
0 Kudos
Reply