how can I use lvgl7 when using version 1.8?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can I use lvgl7 when using version 1.8?

1,486件の閲覧回数
ameng
Contributor I

When I use the lvgl8 version, the screen refresh rate is relatively low.

When I switch back to lvgl7, the refresh rate goes up,

so I still want to use lvgl7, but the guider 1.8 version does not have the lvgl project template.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,456件の閲覧回数
WenbinYuan
NXP Employee
NXP Employee

Hi @ameng,

 

Since the LVGL V7.10.1 in GUI Guider has seen minimal updates in recent releases, you can effectively utilize GUI Guider V1.7.2 to construct V7 projects that include all available features.

 

Best Regards,

Wenbin 

0 件の賞賛
返信

1,434件の閲覧回数
ameng
Contributor I
Thank you. Because version 1.8 has the function of control locking, I want to use this function. Thank you. This software is very good.
0 件の賞賛
返信