guiguider project compiling simulator failed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

guiguider project compiling simulator failed.

1,356件の閲覧回数
Winters
Contributor I

guiguider v1.9.0 on win11 

error when I run the simulator:

Preparing widgets...

Cleaning generated screen files...
Generating C code...
Compiling simulator...

mingw32-make: *** No rule to make target 'C:/Users/Administrator/Desktop/Project/Transplant/transplant/lvgl-simulator/gg_external_data/freemaster/connect_utils.c', needed by 'build/object/connect_utils.o'. Stop. mingw32-make: *** Waiting for unfinished jobs....

Compilation failed!
 

The path in build/object/connect_utils.o is not consistent with the actual project path(which is D:\Project\Transplant\...\transplantV0.90.20250410\lvgl-simulator\build\object)

Snipaste_2025-04-16_10-31-14.pngSnipaste_2025-04-16_10-30-58.png

How can I solve this problem.

 

0 件の賞賛
返信
1 返信

1,312件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Winters 

Can you share your project?

So that i can reproduce this issue.

BR

Harry

0 件の賞賛
返信