bin type font usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bin type font usage

Jump to solution
3,601 Views
frozen
Contributor III

I use NXP Imx RT1170 series mcu and I want to use font as a bin format. How could that possible ?

I see there is a source file as lv_binfont_loader.c but this file is not in the latest tag, it exists in master branch. Why the tag does not include this file ? Is it still in progress ?

I have downloaded offline lvgl font converter and have got bin font file with script. After that I have written this bin file into flash's spesific address and used below functions but I could not see anything in screen. I am open any advice.

lv_font_t my_font;
lv_binfont_load(&my_font,"F:/font.bin");
static lv_style_t font_style;
lv_style_init(&font_style);
lv_style_set_text_font(&font_style, &my_font);

lv_obj_t *label_zh = lv_label_create(ui->screen);
lv_obj_align(label_zh, LV_ALIGN_BOTTOM_MID, 0, 0);
lv_obj_add_style(label_zh, &font_style, 0);
lv_label_set_text(label_zh, "china font");

0 Kudos
Reply
1 Solution
3,518 Views
frozen
Contributor III

thanks @WenbinYuan ,

I preferred to add the function only to lv_font_loader.c file. Then I could use font from bin file.

View solution in original post

2 Replies
3,533 Views
WenbinYuan
NXP Employee
NXP Employee

Hi @frozen,

 

The lv_binfont_loader.c exist in LVGL master branch means it's a new feature of V9.0 which is not released, and GUI Guider only support released version of LVGL (V1.6.1 with LVGL V8.3.5).

And this feature may need other support, check the PR 5333 to get more details if you want use this feature in V8.3.5.

 

Best Regards,

Wenbin

0 Kudos
Reply
3,519 Views
frozen
Contributor III

thanks @WenbinYuan ,

I preferred to add the function only to lv_font_loader.c file. Then I could use font from bin file.