Wrong positioning of DClock widget.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wrong positioning of DClock widget.

1,369 Views
Rino
Contributor II

Hello, 


I found a problem with the positioning of the widget, which is partly related to the size not so much of the displayed time, but the size of the widget itself.

Here are two examples: 

1. The clock on the device is displayed ok, but in the GUI Guider the displayed clock is shifted (theoretically, the blue frame from the selection is in the correct place).

Dclock_pos_1.jpg

2. Example in the other direction, in GG it's ok, the problem with the shift is on the device.

Dclock_pos_2.jpg

Interestingly, by reducing the size of the widget (I don't change the font size or the font itself), it looks like this in GG, but on the device it displays correctly in the middle of the screen (Picture below).

Rino_0-1680181878693.png

Configuration information:
Guider GUI version 1.5.0-GA,
built-in fonts (acme-regular selected),
target device (temporarily) Devboard RT1060-EVK

0 Kudos
Reply
1 Reply

1,338 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

We release new version of Gui Guider (GUI Guider v1.5.1 RC2 )  that we corrected several errors, I suggest that you import your project to this new program to check if this type of error has been corrected.