Tofu characters occur only in widgets

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tofu characters occur only in widgets

Jump to solution
4,770 Views
HSUJK923100
Contributor I

Tofu characters occur only in widgets.


I am using GUI Guider Ver 1.6.1.
If I use labels and use the Arial font for ä ö ü in German, it appears fine.
However, I have run a simulation using the widget list and roller and typing German. Tofu characters occur. It is very troubling.

In other words, as far as I can ascertain, the following is the problem.
1) The tofu characters do not appear in the label, but when I use the widget, the tofu characters appear.
2) The Arial font supports multiple languages, so the font is not the cause.

I would like you to try it too.
Is there a solution?

0 Kudos
Reply
1 Solution
4,754 Views
WenbinYuan
NXP Employee
NXP Employee
0 Kudos
Reply
3 Replies
4,743 Views
HSUJK923100
Contributor I

Thanks for the response. If I want to type German in the widget, I will create a label with the same font size. But I think this condition is a glitch.
Will it be improved in the version update?

0 Kudos
Reply
4,735 Views
WenbinYuan
NXP Employee
NXP Employee

Hi @HSUJK923100 ,

 

Yes, you are right this is a problem and will fixed in next version, so the solution given is just a workaround.

Is this way worked with German? I haven't try it with other language.

 

BR,

Wenbin

0 Kudos
Reply
4,755 Views
WenbinYuan
NXP Employee
NXP Employee
0 Kudos
Reply