Tofu characters occur only in widgets

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Tofu characters occur only in widgets

跳至解决方案
4,777 次查看
HSUJK923100
Contributor I

Tofu characters occur only in widgets.


I am using GUI Guider Ver 1.6.1.
If I use labels and use the Arial font for ä ö ü in German, it appears fine.
However, I have run a simulation using the widget list and roller and typing German. Tofu characters occur. It is very troubling.

In other words, as far as I can ascertain, the following is the problem.
1) The tofu characters do not appear in the label, but when I use the widget, the tofu characters appear.
2) The Arial font supports multiple languages, so the font is not the cause.

I would like you to try it too.
Is there a solution?

0 项奖励
回复
1 解答
4,761 次查看
WenbinYuan
NXP Employee
NXP Employee
0 项奖励
回复
3 回复数
4,750 次查看
HSUJK923100
Contributor I

Thanks for the response. If I want to type German in the widget, I will create a label with the same font size. But I think this condition is a glitch.
Will it be improved in the version update?

0 项奖励
回复
4,742 次查看
WenbinYuan
NXP Employee
NXP Employee

Hi @HSUJK923100 ,

 

Yes, you are right this is a problem and will fixed in next version, so the solution given is just a workaround.

Is this way worked with German? I haven't try it with other language.

 

BR,

Wenbin

0 项奖励
回复
4,762 次查看
WenbinYuan
NXP Employee
NXP Employee
0 项奖励
回复