The code generated by guiguider is incorrect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The code generated by guiguider is incorrect

1,791件の閲覧回数
CloudC
Contributor I
  • I made an UI in Gui-Guider-1.5.1-GA and generated code that failed, like this:

    CloudC_0-1688703995417.png
    • So I clicked on code viewer and looked for errors in the generated code.

    • You can see that the variable name in the above code is different from the variable name used belowCloudC_1-1688704204967.png

       

    • But I can only look at the code and not modify it, so I can only port it to my project code and modify it instead of continuing the simulation.
タグ(1)
0 件の賞賛
返信
1 返信

1,773件の閲覧回数
zongchunyu
NXP Employee
NXP Employee

Hello CloudC,

 

Thank you for reporting this issue. this issue will be fixed in the next GUI Guider release.

 

Best Regards

Zongchun

 

0 件の賞賛
返信