How to use MsgBox in Gui Guider? Suspect there's a software crash if using this widget!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use MsgBox in Gui Guider? Suspect there's a software crash if using this widget!

812 次查看
ChesterLee
Contributor II

Dear NXP Gui-Guider,

This time when I used MsgBox in Gui Guider v1.8.1 and opened simulation, the simulator had crashed before it displayed contents.

I made a MsgBox and set it a HiddenFlg. However I have no idea whether it's correct to use this widget like this.

ChesterLee_0-1732849200762.png

 

I'd really appreciate it if you have any solutions or demos about how to use MsgBox. It'll help me a lot!

Besides, the MsgBox seems that its sub-widget position cannot be set, like I want to set it in middle. Is there any soluton to this?

Tks!

Chester

标记 (3)
0 项奖励
回复
1 回复

781 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

May I ask which chip you are using?

I created a  MsgBox in Gui Guider v1.8.1, and the simulator can run normally.

Can you provide your project? So I can reproduce this issue.

The  sub-widget position in MsgBox cannot be set, you can import the generated code into the IDE and manually modify the relevant code.

BR

Harry

0 项奖励
回复