How to use GUI Guider to generate bin file fonts?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use GUI Guider to generate bin file fonts?

ソリューションへジャンプ
7,881件の閲覧回数
White1
Contributor I

Hello,
may I ask if you could help me: In GUI Guider,I found that only fonts can be generated as C files,Can you add an option to generate bin file fonts? 
At present, BIN files can be generated on the LVGL official website, but when ported to the project generated by GUI Guider, there may be inconsistent font height display issues,May I ask if there is a solution.
I hope to add a tool for generating bin file fonts in the next version!
Thanks!

0 件の賞賛
返信
1 解決策
7,769件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @White1,

This is a great suggestion. I will share this idea internally with the GUI Guider team. In the end, it is up to them to see if this feature is worth implementing on future releases of GUI Guider, but I believe it would be a great addition to the tool!

Thanks for your suggestions.

BR,
Edwin.

元の投稿で解決策を見る

2 返答(返信)
7,770件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @White1,

This is a great suggestion. I will share this idea internally with the GUI Guider team. In the end, it is up to them to see if this feature is worth implementing on future releases of GUI Guider, but I believe it would be a great addition to the tool!

Thanks for your suggestions.

BR,
Edwin.

7,744件の閲覧回数
White1
Contributor I
Thanks for your answer.
If this feature is implemented in future versions, I will be able to store the fonts binary like images binary in XIP FLASH and not have to update the binary every time when updating software code, which will greatly save program update time.
0 件の賞賛
返信