GuiGuider output for STM32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GuiGuider output for STM32

2,473件の閲覧回数
vladi553
Contributor I

The generated С source files (GuiGuider v1.4.1)  indicate that it can be used with NXP products only . Does it mean it cannot be used with STM32 (for example, the files hardware locked for NXP MCU) ?

 
0 件の賞賛
返信
2 返答(返信)

2,459件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @vladi553 

 

Yes, GUI Guider is development for NXP products.

 

BR

Alice

0 件の賞賛
返信

2,446件の閲覧回数
vladi553
Contributor I

OK, thanks. Is it true: GUI guider can only support simulator and NXP development boards as output? Can the user to generate a code for DIY custom boards, where the connection to the TFT must be defined? We also need to write some code to interact with custom TFT. This problems solve by 'porting' section of LVGL help. I configure a small project for simulator and it working well. But how to prepare it for my custom PCB?

 
0 件の賞賛
返信