Gui Guider: no widgets to select from

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gui Guider: no widgets to select from

2,617件の閲覧回数
HansDampf
Contributor I

Dear all,

 

I am new to Gui Guider, downloaded the current version for Linux (Version: 1.8.0-GA ). I am on Ubuntu 22.04, on X86. When start a new project, with simulator target or RT1052, no widgets are shown.

 

I watched some videos about the Gui Guider, there are always the widgets on the left side. As well as in this instructions

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Tool-Step-By-Step-Guider-of-using-GUI-Gu...

the left side of the GUI Guider is full of widgets. But not so on my installation. Is there a secret switch to enable the widgets? Or a bug on the Linux version of the 1.8.0?

 

Thanks

0 件の賞賛
返信
2 返答(返信)

2,584件の閲覧回数
HansDampf
Contributor I

Hi Edwin,

thanks for the quick reply. That was the secret, found it and it works. Great.

 

0 件の賞賛
返信

2,595件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @HansDampf,

With the latest version of GUI Guider, the Widgets panel on the left side now shows the "placed" widgets on each screen, rather than displaying the widget list. 

Now, the widget list can be opened from the "widget" icon on the top left area below UI Editor:

EdwinHz_0-1722881771815.png

Click on it, then click the "Expand" button and you will see all of the new widget list:

EdwinHz_1-1722881866954.png

 

BR,
Edwin.