GUI guider compile error:'SDL2/SDL.h' file not found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GUI guider compile error:'SDL2/SDL.h' file not found

8,520件の閲覧回数
richen
Contributor I

How to figure out the compile error : 'SDL2/SDL.h' file not found

Use MAC OS 12.6 and latest guy guider version.

0 件の賞賛
返信
5 返答(返信)

8,507件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

Hi  richen

  Is your computer architecture arm64?  In response to this problem, I suggest that you can install SDL with source code. Please ensure the install path is /usr/local.  Since the current version is not yet supported by M-core laptops, Some functions will have problems. it's predictable. BTW, We will officially support the ARM64 M-core Mac laptop in the next release(1.6.0). 

BR

Liubin

0 件の賞賛
返信

7,944件の閲覧回数
application_ninja
Contributor V

Any update on this? Still a problem on Gui Guider 1.6.1 with a M-Core Mac...

0 件の賞賛
返信

7,935件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

Hi @application_ninja 

 Please install the SDL based on the steps:

Capture.PNG

 

Thanks

Liubin

5,867件の閲覧回数
lizm0712
Contributor I
it useful,thanks!
0 件の賞賛
返信

7,916件の閲覧回数
application_ninja
Contributor V

This worked, thank you!

0 件の賞賛
返信