GUI GUIDER 1.9.0 : create project error "download is failed"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI GUIDER 1.9.0 : create project error "download is failed"

Jump to solution
8,228 Views
Loic128
Contributor II

Hello,

When I try to create a project with GUI GUIDER (1.9.0 or 1.8.1)  it finished with an error :

"Download is failed, please check your network"

Since I successed to login in GUI GUIDER, I don't think my network is the problem.

What could be the problem?

Thanks

 

0 Kudos
Reply
1 Solution
8,140 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Loic128 

I haven't set up a proxy.

Can you try to change to another network?

BR

Harry

View solution in original post

0 Kudos
Reply
7 Replies
8,203 Views
Loic128
Contributor II

Hi @Harry_Zhang ,

Ok not working for me.

I will try to uninstall and reinstall.

Does it exists an offline version that don't need the network to run ?

Thanks

0 Kudos
Reply
8,192 Views
Loic128
Contributor II

Still the create project error "download is failed please check your network" after uninstall reinstall.

Can we configure the proxy setting somewhere in GUI GUIDER ?

Thanks

0 Kudos
Reply
8,179 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Loic128 

I disconnected the network, and the project can still be successfully created.

Harry_Zhang_0-1739933787755.png

BR

Harry

0 Kudos
Reply
8,161 Views
Loic128
Contributor II

Hi @Harry_Zhang ,

Thank you for your support,

Maybe the first time after install it needs to download things when create project and not after ?

If I disconnected the network I have directly the error "dowload is failed please check your network". 

If I don't disconnected the network I have this error after about 20secondes.

I try to add an exception in firewall but still not works.

Maybe a proxy configuration to set ? Where can I set proxy configuration ?

Thanks, 

0 Kudos
Reply
8,141 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Loic128 

I haven't set up a proxy.

Can you try to change to another network?

BR

Harry

0 Kudos
Reply
8,024 Views
Loic128
Contributor II

Hi @Harry_Zhang ,

With another connection that do not have proxy it's ok, I successfuly create the first project.

After this first project creation, I can create projects with the connection that have proxy without issue.

I think what happened with proxy connection is that I can login in GUI GUIDER with the browser window but GUI GUIDER can't download the things he need at the first project creation.

Thanks

 

0 Kudos
Reply
8,207 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Loic128 

I tested the GUI GUider-1.9.0.

I can successfully create a project.

Please refer to the image.

Harry_Zhang_0-1739874269142.png

BR

Harry

0 Kudos
Reply