Error popup when login

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error popup when login

1,511件の閲覧回数
daniJVV
Contributor III

When I login with my credentials, a pop-up error is shown with this message:

Unhandled Error
TypeError: Object has been destroyed
at EventEmitter.<anonymous> (C:/nxp/GUI-Guider-1.8.1-GA/resources/app.asar/electron_main_utils/IPC/loginIPC.js:54:15)
at EventEmitter.emit (node:events:527:28)

 

The login is correct and I can use GUI Guider normally, but every few days I need to relogin again, because the credentials are saved only this time.

 

Is it a known bug?

 

Thank you

0 件の賞賛
返信
2 返答(返信)

1,475件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @daniJVV 

Every 7 days, you need to log in to your GUIGUIDER account again.

BR

Harry

0 件の賞賛
返信

1,450件の閲覧回数
醒时笑
Contributor I
I created a tileview control in GUI Guider v1.8.1, and when the number of tiles created is more than ten, there is a problem. When setting the horizon direction, the fifth tile displays the last tile. In the vertical direction, two tiles will appear glued together. What is the reason for this?
0 件の賞賛
返信