Designing a Custom Slider

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Designing a Custom Slider

跳至解决方案
2,325 次查看
db1845
Contributor I

Using GUI-Guider v1.9.1, I'm trying to create my own slider. I've easily added the desirable background image but I want to add a different knob to it as my customer desires. I'm just getting a square that only just exceeds the boundaries of the slider when I'm trying to use an image that is a long thin rectangle.

I must be missing something obvious but the only size I can see controls the main element even when the knob is selected on the 'Parts and State' section.

Any assistance greatly appreciated

Screenshot.jpg

 

0 项奖励
回复
1 解答
2,286 次查看
db1845
Contributor I

So, I can see plenty of people have looked at this post but not answered which makes me think it could be a common issue. I’ve done a workaround which keeps me going for now.

Instead of a long thin rectangle, I’ve produce a square that is transparent with the same rectangle in the centre. I’ve then made a slider that is completely transparent apart from the square knob. Underneath this slider I’ve then added an image which is my colour band. This works exactly how I’d like but I’m sure there must be a cleaner solution?

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,287 次查看
db1845
Contributor I

So, I can see plenty of people have looked at this post but not answered which makes me think it could be a common issue. I’ve done a workaround which keeps me going for now.

Instead of a long thin rectangle, I’ve produce a square that is transparent with the same rectangle in the centre. I’ve then made a slider that is completely transparent apart from the square knob. Underneath this slider I’ve then added an image which is my colour band. This works exactly how I’d like but I’m sure there must be a cleaner solution?

0 项奖励
回复
2,224 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @db1845 

Thank you for your message. We will improve this feature in the future.

BR

Harry

0 项奖励
回复