Can't log in and use NXP GUI GUIDER 1.9.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't log in and use NXP GUI GUIDER 1.9.0

1,222件の閲覧回数
Loic128
Contributor II

Hello,

When starting NXP GUI GUIDER there is a blocking window that require to log in. When I try to log it ends by displaying an error : "login check failed, please login again" .

So it's impossible to use the software because the log in window is blocking. I am sure my log user name and password are good because I log successully in the nxp website .

Any idea ?

Thanks

5 返答(返信)

161件の閲覧回数
tombuil
Contributor II

I also have allot problems with GUI guider login.

It does not store my credentials.

I have allot timeouts while login, my internet connection is perfect.

It is very frustrating. I hate using GUI guider JUST because of the login **bleep**.

And now also 2 factor auth is mendatory, making my frustration only bigger.

 

Why do we have to login for using this software at all.... I hate it.

0 件の賞賛
返信

1,157件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello @Loic128  and @mark2 ,
The issue was commented to the internal team, and we are working on it. When I have more information, I will, get back to you as soon as possible.
BR
Habib.

0 件の賞賛
返信

1,168件の閲覧回数
Loic128
Contributor II

Update :  now I succeed to login in GUI GUIDER but when I try to create a project it ends with an error message : "Download is failed, please check your network"

So not completely solved ?

0 件の賞賛
返信

1,113件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello @Loic128,

Can you test run the GUI Guider as admin? if this does not solve the problem, can you disable the firewall and try the same?

BR
Habib

0 件の賞賛
返信

1,210件の閲覧回数
mark2
Contributor III

Same problem here.

0 件の賞賛
返信