Hello,
When starting NXP GUI GUIDER there is a blocking window that require to log in. When I try to log it ends by displaying an error : "login check failed, please login again" .
So it's impossible to use the software because the log in window is blocking. I am sure my log user name and password are good because I log successully in the nxp website .
Any idea ?
Thanks
I also have allot problems with GUI guider login.
It does not store my credentials.
I have allot timeouts while login, my internet connection is perfect.
It is very frustrating. I hate using GUI guider JUST because of the login **bleep**.
And now also 2 factor auth is mendatory, making my frustration only bigger.
Why do we have to login for using this software at all.... I hate it.
Update : now I succeed to login in GUI GUIDER but when I try to create a project it ends with an error message : "Download is failed, please check your network"
So not completely solved ?
Hello @Loic128,
Can you test run the GUI Guider as admin? if this does not solve the problem, can you disable the firewall and try the same?
BR
Habib
Same problem here.