Arduino IDE and LGVL Function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Arduino IDE and LGVL Function

1,869件の閲覧回数
allacmc
Contributor I

I would like to export the GUI BUILDER files and use them in the Arduino IDE.

Which lvgl function do I call to initialize the app made in the GUI Builder?

What files do I have to change considering that in the Arduino IDE I need to have all the files in the same directory without folders and subfolders?

Could anyone help me in this regard?

0 件の賞賛
返信
1 返信

1,815件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that it is a large project to port the LVGL to Arduino IDE.

BR

XiangJun rong

0 件の賞賛
返信