why does the left part of curve in Oscillosope disappear when using CAN communication?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why does the left part of curve in Oscillosope disappear when using CAN communication?

ソリューションへジャンプ
1,613件の閲覧回数
ChenBowen
Contributor II

阶跃最高能过6.PNG

Dear Expert:

    I am using Freemaster2.5, Why does the left part of curve in Oscillosope disappear when using CAN communication?   And more, the curve sometimes suddenly  stops for a second and then moves on, making the curve strange as expected.    

    If using JTAG communication, these issues all resolve , but we need to use CAN in project.

 

 

 

 

0 件の賞賛
返信
1 解決策
1,593件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,

most probably, this is caused by a fact that CAN communication is faster and there is a limited number of points configured for the Oscilloscope graph. 

Go to oscilloscope properties and see the "Buffer" settings (I do not have a screenshot for old version 2.5). The number set there defines the maximum number of points the graph will be able to handle. You can increase this number.

Also, most probably, you have the Period set to 0ms (fastest possible). This means that the fast CAN is able acquire the maximum number of points in graph quicker than over a serial line. If you would set the period to 10ms or so, both CAN and serial would be sampling at the same speed and the graph would behave the same.

Regards,
Michal 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,594件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,

most probably, this is caused by a fact that CAN communication is faster and there is a limited number of points configured for the Oscilloscope graph. 

Go to oscilloscope properties and see the "Buffer" settings (I do not have a screenshot for old version 2.5). The number set there defines the maximum number of points the graph will be able to handle. You can increase this number.

Also, most probably, you have the Period set to 0ms (fastest possible). This means that the fast CAN is able acquire the maximum number of points in graph quicker than over a serial line. If you would set the period to 10ms or so, both CAN and serial would be sampling at the same speed and the graph would behave the same.

Regards,
Michal 

 

0 件の賞賛
返信
1,588件の閲覧回数
ChenBowen
Contributor II

Thank you !

0 件の賞賛
返信