freemaster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freemaster

18,448 Views
fengba_360
Contributor III

want to use Freemaster to monitor and calibrate variables on the S32K144 via CAN, but I'm having trouble effectively configuring the CAN connection in Freemaster (see the illustration). Can you tell me how to solve this problem? Or is there a configuration manual or user guide available?微信图片_20240818192810.png微信图片_20240817144316.png

0 Kudos
Reply
24 Replies

1,061 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

yes the FreeMASTER 3.2.6 supports CAN-FD interfaces from ZLG, IXXAT and Kvaser.

There is a new flexcanfd driver for MCUs supported by NXP MCUXpresso SDK and sample applications making use of this driver. See CAN-FD mode initialized for example in the FRDM-MCXN947 CAN demo.

There is also a FreeMASTER CAN/CAN-FD sample application for Zephyr. 

Regards,
Michal

0 Kudos
Reply

1,057 Views
yang_jacky
Contributor III
OK, I will try It. Thank you~
0 Kudos
Reply

1,055 Views
yang_jacky
Contributor III
Hi,this driver "flexcanfd driver ",how Can I install in my windows 10?
0 Kudos
Reply

1,047 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

the flexcanfd is not a windows driver. It is the MCU low-level C code used internally by FreeMASTER module which handles the communication. One of UART/CAN/RTT/...  low-level communication drivers is selected in freemaster_cfg.h - for example this one for FRDM-MCXN947.

The online documentation of the FreeMASTER MCU module is here. 

Regards,
Michal

0 Kudos
Reply