freemaster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freemaster

18,461 Views
fengba_360
Contributor III

want to use Freemaster to monitor and calibrate variables on the S32K144 via CAN, but I'm having trouble effectively configuring the CAN connection in Freemaster (see the illustration). Can you tell me how to solve this problem? Or is there a configuration manual or user guide available?微信图片_20240818192810.png微信图片_20240817144316.png

0 Kudos
Reply
24 Replies

17,356 Views
iulian_stan
NXP Employee
NXP Employee

Hi @fengba_360 ,

It seems that the corresponding CAN probe driver is either not detected or is not compatible with FreeMASTER.

What CAN adapter are you using ?

Please note that CAN adapter software (driver) should be installed separately of FreeMASTER. 

0 Kudos
Reply

17,342 Views
fengba_360
Contributor III
I am using ZLG CAN card, and freemaster is installed independently. The CAN card driver is also installed independently.
0 Kudos
Reply

17,326 Views
iulian_stan
NXP Employee
NXP Employee

Could you check the following post.

If it does not help, please provide more info about your setup:

  • CAN probe model
  • ZLG driver version
0 Kudos
Reply

17,321 Views
fengba_360
Contributor III

I reinstalled the ZLG CAN driver, and now FreeMASTER can recognize it, but it reports the error shown in the image. Can you tell me how to deal with it?

微信图片_20240820154427.png

0 Kudos
Reply

14,484 Views
yang_jacky
Contributor III
你是怎么解决的?我安装了这个FreeMASTER Commuication Driver 2.0(DSC, S08, S12, S16,MPC).驱动,但还是连接超时,连接不上
0 Kudos
Reply

14,478 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

the ZLG USBCAN-I and USBCAN-II have known issues and may not work with FreeMASTER correctly. I recommend to use newer devices like USBCAN-2E-U, or 4E-U. 

Anyway, when all attempts fail, I would recommend to hook a logic analyzer to CAN RX/TX signals at the microcontroller side and observe if communication reaches the MCU and if it answers (at proper bitrate).

Regards,
Michal

 

0 Kudos
Reply

14,462 Views
yang_jacky
Contributor III
Hi, MichaIH
The devices I am currently using are USBCAN-II and USBCANFD. Is there any way to solve it without replacing the equipment?
0 Kudos
Reply

14,472 Views
yang_jacky
Contributor III
Hi, MichaIH
I currently do not have USB CAN-2E-U or 4E-U devices. Can USB CANFD devices be used?
0 Kudos
Reply

14,465 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello support of USBCANFD device is now under development along with adding support of CAN-FD transport protocol. We plan to release it by end of June as new experimental feature.

Anyway, you can still try the USBCAN device and try to observe the bus (and bit timing) using a logic analyzer or oscilloscope. The issues I talked about with USBCAN are causing the FreeMASTER to crash of hang. If you can press the "Test Connection" button without a crash, then, I think, the USBCAN device could work.

There is a LED on the USBCAN device - it shall flash when you press the Test Connection in the FreeMASTER - that would be a good indication if a CAN frame is transmitted or not.

Regards,
Michal

 

0 Kudos
Reply

14,460 Views
yang_jacky
Contributor III
Hi, MichaIH
When the "Test Connection" button is pressed, the "SYS" LED and "CAN1" channel LED on the USBCAN-II device will flash red for 0.5ms before returning to green. Finally, a warning dialog box pops up, displaying 'Timeout when waiting for the CAN/LIN response (no data received)'
0 Kudos
Reply

14,451 Views
MichalH
NXP Apps Support
NXP Apps Support

I think (not sure) that flashing the red LED is actually good indication that FreeMASTER attempted to send a frame, but it was not acknowledged by anyone on the CAN bus. 

To me it seems the target board does not receive the frame - either because its CAN module is not initialized properly or because the bit-rates do not match. You can double check by putting a breakpoint to a CAN reception routine FMSTR_RxCan() - to see if this function is ever called. If yes, then good the communication works at least somehow. If not, then there is a problem in configuration or bus termination. Make sure the CAN bus is properly terminated by 120ohm resistors on both sides (or at least one side if a wire is short). 

Are you trying to use a CAN example application or your own application? It would be good to try the example first.

 

Regards,
Michal

0 Kudos
Reply

14,443 Views
yang_jacky
Contributor III
Yes, I want to try to use a CAN example application. And How can I get it?
0 Kudos
Reply

14,396 Views
iulian_stan
NXP Employee
NXP Employee

Hi @yang_jacky,

Please find attached an example for S32K144 using FreeMASTER Driver over UART.

This project was build using:

Note: we do not have a planned updates on FreeMASTER Driver for S32K1, so I integrated manually the latest version of the driver.

It uses CAN0 instance @ 500 Kbps (tested with Vector VN1610):

CAN1.png

 

I also included a sample FreeMASTER project that reads a demo variable and plots inside an Oscilloscope chart.

CAN2.png

 

Hope it helps.

0 Kudos
Reply

14,381 Views
yang_jacky
Contributor III
OK, I will try it. thank you very mush.
0 Kudos
Reply

14,443 Views
yang_jacky
Contributor III

Hi,MichaIH


When I use the CANTest tool, the baud rate is set to 500kbps, and the CANTest tool can correctly receive CAN messages sent by the device. When using the FreeMaster tool, the Bit rate is 500KB. May I ask if the baud rate set by the CANTest tool and the Bit rate set by FreeMaster are in the same unit. Is there a difference between baud rate and bit rate?


_cgi-bin_mmwebwx-bin_webwxgetmsgimg__&MsgID=2430470622228025231&skey=@crypt_c6607432_825280485d809fa82b83dfc8511bae68&mmweb_appid=wx_webfilehelper.jfif_cgi-bin_mmwebwx-bin_webwxgetmsgimg__&MsgID=5482576845431562885&skey=@crypt_c6607432_825280485d809fa82b83dfc8511bae68&mmweb_appid=wx_webfilehelper.jfif_cgi-bin_mmwebwx-bin_webwxgetmsgimg__&MsgID=992743456016068767&skey=@crypt_c6607432_825280485d809fa82b83dfc8511bae68&mmweb_appid=wx_webfilehelper.jfif

0 Kudos
Reply

17,308 Views
iulian_stan
NXP Employee
NXP Employee

In most cases this error code means that FreeMASTER (desktop tool) did not receive a reply from the target board.

You would need to check whether CAN interface and FreeMASTER Driver are properly configured.

If you are using SDK to configure the CAN, you may need to disable transmission abort mechanism (see this thread for more info). 

0 Kudos
Reply

14,499 Views
yang_jacky
Contributor III
I encountered the same problem.And I have already installed the FreeMASTER Commuication Driver 2.0(DSC, S08, S12, S16,MPC).When I click the 'Test Connection' button, the warning 'Timeout when waiting for the CAN/LIN response (no data received)' still appears. Could you tell me how to deal with it?
0 Kudos
Reply

17,302 Views
fengba_360
Contributor III
Where can I download the FreeMASTER Driver? Could you please provide me with a link?
thanks
0 Kudos
Reply

17,296 Views
iulian_stan
NXP Employee
NXP Employee

It's available on FreeMASTER's home page in downloads section. Here's a direct link.

Capture.PNG

 

If you are using S32 Design Studio, it is already included in S32K1xx development package - you can find it in `C:\NXP\S32DS.3.5\S32DS\software\FreeMASTER_Serial_Communication_Driver_V2_0`.

I would also recommend checking the following post - it explains UART configuration, but the same flow applies in case of CAN communication.

0 Kudos
Reply

8,269 Views
yang_jacky
Contributor III
Hi, I want to ask  a question is that,Last time Michelle mentioned that a FreeMaster version will be released in October 2025, supporting ZLG's CANFD. Has this version been released yet? If it has already been released, where can I download it?
0 Kudos
Reply