Wrong FreeMASTER Download Version?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wrong FreeMASTER Download Version?

2,706 Views
MaWi
Contributor I

Hi,

on the website

https://www.nxp.com/design/software/development-software/freemaster-run-time-debugging-tool:FREEMAST...

FreeMASTER is available as software download. But when I install it, it says Version 3.1.3.8 in the About... dialog. This is in contrast to the version number 3.1.4 stated on the download website.

Something is wrong here...  

0 Kudos
Reply
3 Replies

2,698 Views
iulian_stan
NXP Employee
NXP Employee

Hi @MaWi,

I just checked the link.

Capture.PNGCapture.PNG

The downloaded executable shows version 3.1.4.5.

Capture.PNGCapture.PNG

 

Same version is displayed in About window.

Capture.PNGCapture.PNG

 

In case you have multiple installers of FreeMASTER please make sure that:

  1. The downloaded file has the right version (figure 2)
  2. Installation is finished successfully

Kind regards,
Iulian

0 Kudos
Reply

2,690 Views
MaWi
Contributor I

Strange...

I downloaded following file again:

  • IDE AND BUILD TOOLS

    FreeMASTER tool 3.1 – Windows installerFEATURED

    EXERev 3.1.4Mar 24, 2022348.0 MBFMASTERSW31-EXE
    Sign in required
     
    Then I double checked the version of the exe file in my download folder.
    MaWi_0-1652360214380.pngMaWi_0-1652360214380.png

     

    It is still version 3.1.3.8, no matter how often I try again...

    I am confused.

     
     
     
0 Kudos
Reply

2,678 Views
iulian_stan
NXP Employee
NXP Employee

That's strange indeed. I will follow up with site management team and will post updates once I get some feed-back.

0 Kudos
Reply