Wrong FreeMASTER Download Version?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wrong FreeMASTER Download Version?

2,731件の閲覧回数
MaWi
Contributor I

Hi,

on the website

https://www.nxp.com/design/software/development-software/freemaster-run-time-debugging-tool:FREEMAST...

FreeMASTER is available as software download. But when I install it, it says Version 3.1.3.8 in the About... dialog. This is in contrast to the version number 3.1.4 stated on the download website.

Something is wrong here...  

0 件の賞賛
返信
3 返答(返信)

2,723件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @MaWi,

I just checked the link.

Capture.PNG

The downloaded executable shows version 3.1.4.5.

Capture.PNG

 

Same version is displayed in About window.

Capture.PNG

 

In case you have multiple installers of FreeMASTER please make sure that:

  1. The downloaded file has the right version (figure 2)
  2. Installation is finished successfully

Kind regards,
Iulian

0 件の賞賛
返信

2,715件の閲覧回数
MaWi
Contributor I

Strange...

I downloaded following file again:

  • IDE AND BUILD TOOLS

    FreeMASTER tool 3.1 – Windows installerFEATURED

    EXERev 3.1.4Mar 24, 2022348.0 MBFMASTERSW31-EXE
    Sign in required
     
    Then I double checked the version of the exe file in my download folder.
    MaWi_0-1652360214380.png

     

    It is still version 3.1.3.8, no matter how often I try again...

    I am confused.

     
     
     
0 件の賞賛
返信

2,703件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

That's strange indeed. I will follow up with site management team and will post updates once I get some feed-back.

0 件の賞賛
返信