Vector VN1630A LIN Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vector VN1630A LIN Support

3,455件の閲覧回数
WattYao
Contributor I

I want to use freeMaster over lin communication, but it only supports nican. Can support device: vector vn1630A?

0 件の賞賛
返信
2 返答(返信)

3,451件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear WattYao,

yes, FreeMASTER-over-LIN is still a bit experimental feature as it needs pretty specific support on the target side (multi-frame transport layer, diag-class II or III). There were just few users interested in this solution so far, so the PC support has not evolved more than to a single NI USB-to-LIC device support.

The situation with FreeMASTER-over-CAN is different. There are many users and wide support for different CAN hardware including Vector, HMS Ixxat, Kvaser and others.

Can you tell more about your target application? Do you use NXP LIN communication stack? What is your target platform?

Thanks,
Michal

0 件の賞賛
返信

3,446件の閲覧回数
WattYao
Contributor I

The platform is MC9S12ZVM, there will be no CAN transceiver in mass production, only LIN communication.

0 件の賞賛
返信