Vector VN1630A LIN Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vector VN1630A LIN Support

3,409 Views
WattYao
Contributor I

I want to use freeMaster over lin communication, but it only supports nican. Can support device: vector vn1630A?

0 Kudos
Reply
2 Replies

3,405 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear WattYao,

yes, FreeMASTER-over-LIN is still a bit experimental feature as it needs pretty specific support on the target side (multi-frame transport layer, diag-class II or III). There were just few users interested in this solution so far, so the PC support has not evolved more than to a single NI USB-to-LIC device support.

The situation with FreeMASTER-over-CAN is different. There are many users and wide support for different CAN hardware including Vector, HMS Ixxat, Kvaser and others.

Can you tell more about your target application? Do you use NXP LIN communication stack? What is your target platform?

Thanks,
Michal

0 Kudos
Reply

3,400 Views
WattYao
Contributor I

The platform is MC9S12ZVM, there will be no CAN transceiver in mass production, only LIN communication.

0 Kudos
Reply