Unable to find FreeMaster 3.0 on PC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to find FreeMaster 3.0 on PC

跳至解决方案
5,933 次查看
rparveez
Contributor II

Hi,

I completed the installation process of FreeMaster 3.0 but I was not able to find the application. When I tried to reinstall the application it popped up a message saying already installed and pointed to a folder "NXP FreeMaster". However, that folder did not have correct installation structure neither it had uninstall.exe file (instead had a uninstall.jar file). I deleted the entire folder and tried to install again but still it pops the same abort message (Already Installed and pointing to folder location "NXP FreeMaster") but that folder no longer exist now. 

I need help in reinstalling FreeMaster 3.0 on my PC.

0 项奖励
回复
1 解答
5,911 次查看
iulian_stan
NXP Employee
NXP Employee

Hi @rparveez,

There are some additional registry entries used by the installer that are located at

C:\Program Files (x86)\Zero G Registry\.com.zerog.registry.xml

In case this file contains a FreeMASTER entry in <products> list the, back up the file and remove it from the disk. Relaunch the installer.

 

Note: If FreeMASTER is the only product it the mentioned registry file, it is safe to completely remove the file (without backup) as it will be recreated automatically during installation process.

在原帖中查看解决方案

3 回复数
5,912 次查看
iulian_stan
NXP Employee
NXP Employee

Hi @rparveez,

There are some additional registry entries used by the installer that are located at

C:\Program Files (x86)\Zero G Registry\.com.zerog.registry.xml

In case this file contains a FreeMASTER entry in <products> list the, back up the file and remove it from the disk. Relaunch the installer.

 

Note: If FreeMASTER is the only product it the mentioned registry file, it is safe to completely remove the file (without backup) as it will be recreated automatically during installation process.

4,253 次查看
cucumilo
Contributor I

thank you very much, this solution resolved my problem.

0 项奖励
回复
5,901 次查看
rparveez
Contributor II

Hi @iulian_stan ,

This solution resolved my issues. Thank you.

 

0 项奖励
回复