S32K144 Control motor Kit brush history Freemaster problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 Control motor Kit brush history Freemaster problems

2,811件の閲覧回数
YANMING1
Contributor I

I use S32DS to burn the process code, and then enter the Freemaster control interface, click GO will appear the following problems, there is no error, please tell me how to solve

15571289167_0-1725710661769.png

 

 

0 件の賞賛
返信
2 返答(返信)

2,699件の閲覧回数
YANMING1
Contributor I

Hello Radeks:

Thanks for your answer. According to the self-check on NXP's official website, I found some problems with my software and hardware. Now I can control the motor by pressing buttons, but there are still some problems.
 I can't control the motor speed through the Freemaster panel

YANMING1_0-1727186074384.png

 

0 件の賞賛
返信

2,734件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hello YANMING1,

Unfortunately your screenshot is dificult to read and we do no knw what sw examples do you use.

However I can see that MCAT reports error GD3000 fault (and phase currents).

I guess that problem might be in jumper settings or incorrect connection between S32K144EVB and DEVKIT-MOTORGD board.

Please check that:

  • J107 at S32K144EVB is in position 1-2
    RadekS_0-1726751014993.png
  • J9, J10 and J11 at DEVKIT-MOTORGD board are in position 1-2 and J8 is open
    RadekS_1-1726751256346.png
  • DEVKIT-MOTORGD board is correctly and fully plugged into S32K144EVB
  • You have connected the motor phase wires in correct order (this should not present any problem)
  • You plugged 12V power supply to the DEVKIT-MOTORGD board
    RadekS_2-1726752149597.png
  • you have connected connector with hall sesnors like on picture above (this is related only to sw example with hall sensors)
  • you opened FreeMASTER project from the same project folder that you uploaded into MCU.  
  • you may check also temperature of GD3000 chip. Simply by finger. If it is too hot and you cannot keep finger on chip longer than 2 seconds, the chip might be damaged (e.g. by static discharge, but this is pure speculation). 

For more detail you may look at Getting Started web page .

Best regards

RadekS

 

0 件の賞賛
返信